Icon_Blog-sq

When is Make-Up Air Required for Kitchens?

by Codie Hoffmann |
When is Make-Up Air Required for Kitchens?

Have you ever left a restaurant smelling like you’ve been cooking burgers for hours? If you have, it could be that the restaurant has a make-up air/exhaust system not working correctly. Selecting the correct make-up air solution for your kitchen can be the difference between your customers having an excellent experience or a poor one.

What is make-up air?


Make-up air is the air that is being supplied to a space (a restaurant in this instance) to make up for the exhausted air. This exhausted air in this case is grease or smoke that exits through a hood.

Why is make-up air important?


Building codes require make-up air in kitchens, cafeterias, and similar applications above a specified volume. Section 505 of the International Mechanical Code (IMC) states that “exhaust hood systems capable of exhausting in excess of 400 cfm shall be provided with makeup air.”

Aside from the fact that mechanical codes often require it, make-up air also plays a pivotal role in the function of an exhaust system. In the absence of make-up air, the exhaust fan removes air from the space creating negative pressure. The performance of the exhaust fan can diminish significantly as pressure becomes more negative. You might recognize a familiar example of negative pressure when your doors open difficultly. This increasing negative pressure can drop volume exhausted up to 30%. It reduces the ability to capture grease/smoke by the hood, allowing it to seep into the seating area making for unhappy customers.

Commonly Used Terms

  • Makeup air unit – A unit specifically used to supply, or make-up, for air being exhausted from the space. Make-up air units are mounted on a rooftop, above the ceiling or on a slab in most applications
  • Rooftop unit – A unit in the HVAC system that contains all required components to provide conditioned air in one unit. Generally, they are unable to provide high volumes of outside air to offset exhausted air
  • Louver – A non-mechanical unit mounted in the wall of the building’s exterior to allow airflow into or out of the building while preventing water infiltration


What are the most common options available to make-up the exhausted air?

The make-up air solutions considered for most projects are:

  • Make-up air unit, usually direct-gas or no-heat, that’s interlocked with the exhaust fan
  • Rooftop unit which generally operates independent of the exhaust fan for make-up air
  • Pull make-up air through louver or door without assistance of a fan


The pros and cons of each option

Several factors need to be considered to select the best solution. These include initial cost, operating cost, level of control, and volume exhausted. Each factor needs to be carefully weighed to ensure that the most important needs are covered. The advantages and disadvantages of each make-up air solution follow.

When is Make-Up Air Required for Kitchens-Figure1_
Figure 1


Advantages of make-up air unit that’s interlocked with the exhaust fan (Figure 1)

  • Offers the ability to heat/cool air for the specific needs of the kitchen resulting in energy savings
  • Highest level of control over building pressure because the make-up air is only provided when exhaust fan is active
  • Air is filtered to prevent contaminants from getting into the kitchen


Disadvantages of make-up air unit that’s interlocked with the exhaust fan

  • Make-up air units add additional cost which is in addition to the rooftop unit
  • A larger footprint is required because a make-up air and rooftop unit are required
When is Make-Up Air Required for Kitchens-Figure2_
Figure 2
 

Advantages of using rooftop unit for make-up air (Figure 2)

  • Initial cost savings from installing a single unit instead of a make-up air and rooftop unit
  • Reduced footprint because only one unit is being used


Disadvantages of using rooftop unit for make-up up air

  • Heating and cooling are more than required for the kitchen resulting in additional energy consumption
  • The rooftop unit will need to cycle on/off to maintain building pressure resulting in additional wear and tear on components
When is Make-Up Air Required for Kitchens-Figure3_
Figure 3
 

Advantages of using a louver or opening a door (Figure 3)

  • This solution can be the most cost-effective in certain settings


Disadvantages of using a louver or opening a door

  • Air is generally unfiltered, so there’s no way to keep contaminants out of the kitchen
  • No tempering so the temperature of air entering the building can’t be controlled, potentially causing an uncomfortable condition for occupants
  • This option may violate codes in certain situations


When does it make sense to use a make-up air unit that will be interlocked with the exhaust fan in addition to a rooftop unit?

Restaurant situations that exhaust at or greater than 800 cfm often make sense to use a make-up air unit which is interlocked with the exhaust fan. Accommodating this amount of outdoor air volume with a rooftop unit only is difficult. Similarly, providing 800 cfm or more to the space when the kitchen hood is inactive will cause pressure issues. It requires more complex controls to avoid problems with pressure which would require the rooftop unit to cycle on/off frequently.

Using a louver or door for the make-up air above 800 cfm will not work well either. The air coming into the space is a relatively large volume of untempered and unfiltered air, resulting in a complete lack of control of temperature and air quality in the space. It is possible that this option could violate the IMC code in certain situations. The louver or door option could still meet code under certain circumstances. Much depends on the type of HVAC system or local climate. You should consult with a knowledgeable HVAC engineer. Still, a make-up air unit remains a better option.


Summary


Having make-up air always is a good idea when using a hood to exhaust grease/smoke-laden air. You need make-up air per the IMC, if exhausting more than 400 cfm. Using a rooftop unit to compensate for the exhausted air is common when exhausting less than 800 cfm. The volume is minimal, so the additional pressure and tempering control have a relatively minimal impact. However, a make-up air unit is the best option when supply air is at or above 800 cfm. A make-up air unit in conjunction with a rooftop unit is the best option to bring the space pressure back to neutral or slightly negative. This gives you the ability to temper the air to the specific needs of the kitchen to reduce operating cost. If the exhaust hood rarely runs and the climate is mild, opening a door or using a louver may be a viable option and an opportunity to reduce project cost. Remember, the make-up air solution used could be the difference between a happy customer and a disappointed customer.
Kitchen Ventilation Make-up Air
Join the discussion...
Leave a comment
Reader Comments
Comment by
from
Codie Hoffmann
Codie Hoffmann
Codie Hoffmann
Codie Hoffmann is an Application Engineer Specialist at Greenheck. He has been with Greenheck since 2016 and has held roles in finance, power roof ventilators, louvers, and most recently tempered air products. Currently, he supports the make-up air product line. Codie has a Bachelor of Science degree in business administration from the University of Wisconsin – Stevens Point.
Other Blog Topics
Other Blog Topics