CORPORATE INFORMATION
March, 2025 - Greenheck Awarded Sourcewell Cooperative Contract
Expanding Opportunities in Government Procurement.
July, 2024 - Greenheck Named Winner in ACHR NEWS 2024 Dealer Design Awards
Greenheck was recognized for excellence in product design in the 2024 Dealer Design Awards Program, sponsored by The Air Conditioning, Heating & Refrigeration News magazine.
FANS
September, 2024 - Greenheck Introduces RSQ Hooded Rooftop Fan
New RSQ direct drive rooftop fan, available in supply or exhaust configuration, incorporates mixed flow wheel technology to improve airflow and efficiency, reduce sound, and allow for a more compact design.
September, 2024 - Greenheck Redesigns Upblast Powered Roof Ventilators
Next-Generation features make fans even easier to service.
June, 2024 - Greenheck Expands MultiSPEC™ SP-LP Ceiling Exhaust Fan Line
Greenheck has expanded its MultiSPEC™ SP-LP ceiling exhaust fan line with two new high-performance models.
LOUVERS
April, 2024 - Greenheck Introduces AFL-601 Wind-Driven Rain FEMA Louver
Greenheck’s line of FEMA 361 tornado louvers has expanded with the addition of model AFL-601, the first wind-driven rain FEMA louver to be listed for AMCA 550 High-Velocity Wind-Driven Rain.
DAMPERS
August, 2024 - Greenheck Expands Isolation Damper Line
New HBT-321 Damper Designed for Safety in Critical Leakage Applications.
DEDICATED OUTDOOR AIR SYSTEMS (DOAS)
October, 2024 - Greenheck’s Air-Source Heat Pumps Deliver Energy-Efficient Heating at 0° Fahrenheit
Enhanced Capabilities for Northern Climates.
October, 2024 - Greenheck’s Air-Source Heat Pumps Deliver Energy-Efficient Heating at 0° Fahrenheit
Enhanced Capabilities for Northern Climates.
ROOFTOP UNITS
April, 2025 - Greenheck Launches New Line Of Rooftop Units
Model RT simultaneously controls temperature and humidity to deliver optimized comfort.
MAKE-UP AIR
December, 2024 - Greenheck’s Direct Gas-Fired Make-Up Air Units Now Feature R-454B Refrigerant
Direct gas-fired make-up air units from Greenheck now use R-454B, an A2L refrigerant mandated by the Environmental Protection Agency with low potential to contribute to global warming.
ENERGY RECOVERY VENTILATORS
January, 2025 - Greenheck’s New ERVi Energy Recovery Ventilators Excel in Indoor Spaces
Indoor-Mounted Units Provide 100% Outdoor Air.
July, 2024 - Greenheck Adds New Models to Commercial Multifamily/Residential Energy Recovery Ventilator Line
Greenheck has added three new models to its line of high-performance residential energy recovery ventilators (ERVs) that provide balanced ventilation and improve energy efficiency to ensure projects meet code and exceed indoor air quality expectations.
AIR DISTRIBUTION
February, 2025 - Square Ceiling Diffusers From Greenheck
Models Ensure Uniform Air Distribution.
November, 2024 - Fan-Powered Air Terminal Units From Greenheck
Constant and Variable Volume Models for Energy-Efficient Zone Control.
January, 2024 - New XG-AFL Series Linear Diffusers from Greenheck
Greenheck's XG-AFL Series of architectural high-capacity linear slot diffusers are designed for ceiling and sidewall installation in variable volume or constant volume air distribution systems.
HEALTHCARE LABORATORY CLEANROOM
March, 2024 - Greenheck Introduces Modular Air Distribution Systems for Operating and Imaging Rooms
Diffuser Arrays Simplify Coordination During Design and Installation