QUICK DELIVERY
The shortest possible delivery times on a wide selection of in-stock products.
Greenheck’s Quick Delivery (QD) program is the industry’s most comprehensive offering of commonly requested ventilation equipment. These products are in-stock and ready to ship. This program is backed up by an even larger assortment of configure-to-order products built just for you, in the time frame you need!
Now you can order in-stock Greenheck fans, dampers, louvers, and accessories online.
Which program will work best for me?
Do you need it now? The QD program has more than 1000 of the most in-demand products in stock, ready to ship.
Some products require specific customization to meet the demands of a project. These are built as needed. But this does not translate into long wait times.
Greenheck’s Quick Build (QB) program ensures these products can be manufactured as needed in 1, 3, 5, 10, 15, and 25 day manufacturing cycles.
How do I order?
There are two ways to place a QD order.
1. Contact your local Greenheck representative and have them place the order for you.
2. Order online. This allows you to select the product(s) you want, add it to a shopping cart and place the order yourself, quickly and easily.
When can I get the product I need?
Place your order by 2 p.m., Central Time, Monday through Friday and your order will ship that same day.
Orders received after 2 p.m. will ship the next business day.
QB orders receive before 1 p.m. each business day will ship within the time parameters of the product(s) ordered (1, 3, 5, 10, 15, or 25 days).
Where will it ship from?
Products ship from five distribution centers strategically located across the U.S. This means your product is only a day or two away with ground shipment.
Expedited delivery is possible. Your Greenheck representative can provide you with the details.
Greenheck products are manufactured across the U.S. at six manufacturing locations. Your product will ship from the closest location where the product is built.
Quick freight options are available and if required, our shipping professionals will work with your local representative to ensure prompt delivery.
To view the complete offering of stock and Quick Build products, visit the Quick Delivery ecommerce site or select a specific product category below:
PRODUCT CATEGORIES
IN STOCK
QUICK BUILD
GREENHECK DISTRIBUTION CENTERS
Greenheck products are close to your project site. Our five distribution centers are strategically located across the U.S., which means standard ground transit times are one to two days. You may also pick up your order at the closest warehouse if that is more convenient.