Greenheck will be closed Thursday, July 4th in observance of the July 4th holiday. Please note that shipments on July 5th may incur shipment delays. Full order shipments will resume on Monday, July 8th.
In-stock items ship today if ordered in:
HR : MIN : SEC
Same day shipping on thousands of in-stock items
DETAILS
Designed for inline installations and offering a wide performance range. Fans are used for clean air, sound sensitive, or industrial exhaust air applications.
Use the calculator to determine the Air Exchange (CFM) required to adequately ventilate an area.
Enter information into the fields below to calculate the required airflow per fan.
To calculate the CFM required to adequately ventilate an area, we divide the room volume by the appropriate “Minutes per Change” value.
[CFM] = [Room Volume] / [Min./Chg.]
Airflow (CFM) per Fan
*
Starred items represent required fields.
Calculate Static Pressure (SP)
Use the calculator to determine the amount of static pressure the fan must overcome.
The pressure generated by fans in ductwork is typically very small. An accurate measurement of static presure is critical to proper fan selection however. Static pressure in fan systems is typically less than 2" SP, or 0.072 Psi.
The amount of static pressure that the fan must overcome depends on the air velocity in the ductwork, the number of duct turns (and other resistive elements), and the duct length. For properly designed systems with sufficient make-up air, the guidelines in the table below can be used for estimating static pressure.
Static pressure
*Starred items represent required fields.
Static Pressure Guidelines
Non-Ducted 0.05" to 0.20"
Ducted 0.20" to 0.40" per 100 feet of duct (assuming duct air velocity falls within 1,000 to 1,800 feet per minute)
Important: Static pressure requirements are significantly affected by the amount of make-up air supplied to an area. Insufficient make-up air will increase static pressure and reduce the amount of air that will be exhausted. Remember, for each cubic foot of air exhausted, one cubic foot of air must be supplied.
View as
Sort by
Results per page
Showing0of0results
Shop Greenheck Products
As the worldwide leader in manufacturing high quality air movement, control and conditioning products, Greenheck offers the most comprehensive line of ventilation equipment available including fans, dampers, louvers and fan accessories. Our equipment is used across a variety of commercial, institutional, and industrial buildings in applications from comfort ventilation to manufacturing processes.